Skip to content

Asiakkaamme ja kumppanimme

Fibox arvostaa asiakkaitaan, ja näemme asiakkuudet kumppanuuksina, joiden kesto mitataan vuosien sijaan vuosikymmenissä.

Olemme monessa mukana

Fibox on erikoistunut vaativiin ympäristöihin ja aloihin. Turvaamme kriittiset osat päivästä, vuodesta ja vuosikymmenestä toiseen.

REFERENCES

Previous slide

GLITTERING EIFFEL TOWER

The Fibox MNX range of IP67 polycarbonate weatherproof industrial enclosures is considered ideal for those heavy-duty applications where a robust yet aesthetically pleasing product is required.

That is why the FIBOX MNX range was chosen to house the prestigious lighting scheme on one of the worlds most recognizable and visited landmarks… THE EIFFEL TOWER.

By working closely with the tower’s lighting design team, FIBOX was able to offer a tailored solution exactly to specification. This included a specially moulded cover to optimize light output, and a neutral-coloured base to help make the lighting installation as unobtrusive as possible. In total, 22,000 enclosures were installed, each housing a single lamp. The effect is truly stunning!

 

Utö island

The oldest Fibox enclosures are located in Utö island in Finland. They were installed in 1971.

The Baltic sea offers wide range of harsh conditions that protective enclosures need to face. Cold winters and warm summers with direct UV-radiation. Salty sea makes environment also corrosive therefore Fibox enclosures have been optimal solution for long life time use.

 

 

 

 

 

Incheon Bridge

The Icheon Grand Bridge is South Korea’s longest spanning cable-stayed bridge and the fifth largest in the world.  The bridge was opened in October 2009 and connects Incheon Airport to Songdo.

Fibox enclosure products are being used to control bridge safety applications.

 

 

 

 

 

Next slide

OTA YHTEYTTÄ!

Jos sinulla on kysyttävä, olet kiinnostunut kuulemaan lisää tai haluat tarjouksen, olemme täällä sinua varten. Ota rohkeasti yhteyttä!